Hello,
I hope to know a frame rate as h.264 decode result.
Can I get a result of the decoder output frame rate using gstreamer?
If no, please teach me some method to show a frame rate of h.264 decoder result.
Best regards,
Ishii.
you can find out from log file when you decoding the file, the log file would shows the time and frame number, then you can calculate it.
Hello Xie,
Thank you for your quick response.
As you say, that log file mean to use "GST_DEBUG" and "GST_DEBUG_FILE" option?
If so, which number for GST_DEBUG option will be output the time and frame number?
you just need to play the video using unit test or gstreamer, you can find it.
Hello Joan,
Thank you for your response.
I was able to see it by playing the stream to the end.
Before it, I force stopped it because play time too long.