How to set a YCbCr 8bit data output?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set a YCbCr 8bit data output?

ソリューションへジャンプ
2,223件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm designing a system with i.MX6 processor and planning to output YCbCr 8bit data from IPUx_DISP0_DATAxx.

Are there any rules to use it?

Can I use any bit in DISP0[23:0]?

If so, Please let me know how to set the output bit.

Please clarify,

Sincerely

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,964件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, DISP0[70]  should be used.

~Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,964件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to Table 68 (Video Signal Cross-Reference) of the i.MX6 Datasheet (IMX6DQCEC,

Rev. 3, 02/2014) regarding the mapping of the Display Interface Pins used during various

supported  video interface formats. You may apply to Linux tests, described in section 
“IPU Device Unit test” of Linux Reference Manual.  Also, I hope general considerations in the
next Community thread helps :

"Parallel RGB Displays"

https://community.freescale.com/message/394334#394334

Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,964件の閲覧回数
ko-hey
Senior Contributor II

Hi Yuri

The table means that I can use only DISP0[70] doesn't you?

Or I can use other bit as a data output? (ex, DISP0[15:8])

Which one is correct?

Best Regards,

ko-hey

0 件の賞賛
返信
1,965件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, DISP0[70]  should be used.

~Yuri.

0 件の賞賛
返信