How to set a YCbCr 8bit data output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set a YCbCr 8bit data output?

Jump to solution
2,490 Views
ko-hey
Senior Contributor II

Hi all

I'm designing a system with i.MX6 processor and planning to output YCbCr 8bit data from IPUx_DISP0_DATAxx.

Are there any rules to use it?

Can I use any bit in DISP0[23:0]?

If so, Please let me know how to set the output bit.

Please clarify,

Sincerely

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,231 Views
Yuri
NXP Employee
NXP Employee

Yes, DISP0[70]  should be used.

~Yuri.

View solution in original post

0 Kudos
Reply
3 Replies
2,231 Views
Yuri
NXP Employee
NXP Employee

Please refer to Table 68 (Video Signal Cross-Reference) of the i.MX6 Datasheet (IMX6DQCEC,

Rev. 3, 02/2014) regarding the mapping of the Display Interface Pins used during various

supported  video interface formats. You may apply to Linux tests, described in section 
“IPU Device Unit test” of Linux Reference Manual.  Also, I hope general considerations in the
next Community thread helps :

"Parallel RGB Displays"

https://community.freescale.com/message/394334#394334

Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,231 Views
ko-hey
Senior Contributor II

Hi Yuri

The table means that I can use only DISP0[70] doesn't you?

Or I can use other bit as a data output? (ex, DISP0[15:8])

Which one is correct?

Best Regards,

ko-hey

0 Kudos
Reply
2,232 Views
Yuri
NXP Employee
NXP Employee

Yes, DISP0[70]  should be used.

~Yuri.

0 Kudos
Reply