How to run a none-OS mx28 program on Nand flash ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run a none-OS mx28 program on Nand flash ?

Jump to solution
2,145 Views
9crkzhou
Contributor III

no linux , no uboot, just a LED program.

actually,it is the ODBS of mx28...

how to run it on Nand flash ?

I'v use the MFGTool, while it appeares not running at all.

Labels (2)
0 Kudos
Reply
1 Solution
1,984 Views
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

View solution in original post

0 Kudos
Reply
3 Replies
1,984 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, zhou

     Everytime system power up, boot ROM will be always running first, then it will call plugin to init power, DRAM...there is a file linux.bd in linux-bootlets, I think you can put your test image here, then call it and run it. But you still need to program it into NAND flash, and set system to boot from NAND, then ROM will try to read the image in NAND and run it in DRAM, not sure whether this is what you want.....

0 Kudos
Reply
1,984 Views
9crkzhou
Contributor III

I'm tring to make the OBDS program runing on Nand Flash.it works well in SD card.

but when I flash it into Nand with MFGTool, there no response at all ,and the MFGTool detected the HID compliant Device, which means boot from Nand failed.

0 Kudos
Reply
1,985 Views
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

0 Kudos
Reply