How to run a none-OS mx28 program on Nand flash ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to run a none-OS mx28 program on Nand flash ?

跳至解决方案
3,235 次查看
9crkzhou
Contributor III

no linux , no uboot, just a LED program.

actually,it is the ODBS of mx28...

how to run it on Nand flash ?

I'v use the MFGTool, while it appeares not running at all.

标签 (2)
0 项奖励
回复
1 解答
3,074 次查看
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,074 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, zhou

     Everytime system power up, boot ROM will be always running first, then it will call plugin to init power, DRAM...there is a file linux.bd in linux-bootlets, I think you can put your test image here, then call it and run it. But you still need to program it into NAND flash, and set system to boot from NAND, then ROM will try to read the image in NAND and run it in DRAM, not sure whether this is what you want.....

0 项奖励
回复
3,074 次查看
9crkzhou
Contributor III

I'm tring to make the OBDS program runing on Nand Flash.it works well in SD card.

but when I flash it into Nand with MFGTool, there no response at all ,and the MFGTool detected the HID compliant Device, which means boot from Nand failed.

0 项奖励
回复
3,075 次查看
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

0 项奖励
回复