How to run a none-OS mx28 program on Nand flash ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run a none-OS mx28 program on Nand flash ?

ソリューションへジャンプ
2,160件の閲覧回数
9crkzhou
Contributor III

no linux , no uboot, just a LED program.

actually,it is the ODBS of mx28...

how to run it on Nand flash ?

I'v use the MFGTool, while it appeares not running at all.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,999件の閲覧回数
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,999件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, zhou

     Everytime system power up, boot ROM will be always running first, then it will call plugin to init power, DRAM...there is a file linux.bd in linux-bootlets, I think you can put your test image here, then call it and run it. But you still need to program it into NAND flash, and set system to boot from NAND, then ROM will try to read the image in NAND and run it in DRAM, not sure whether this is what you want.....

0 件の賞賛
返信
1,999件の閲覧回数
9crkzhou
Contributor III

I'm tring to make the OBDS program runing on Nand Flash.it works well in SD card.

but when I flash it into Nand with MFGTool, there no response at all ,and the MFGTool detected the HID compliant Device, which means boot from Nand failed.

0 件の賞賛
返信
2,000件の閲覧回数
9crkzhou
Contributor III

I'v got it , go to see a .bd file ,then you understand everything.

0 件の賞賛
返信