How to remove the SD card read-only mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to remove the SD card read-only mode

跳至解决方案
2,491 次查看
jingyangxie
Contributor V

Hi,all

      I have an imx6q motherboard, when using MicroSD card, the linux always prompts SD card for read-only mode, how can I solve this problem?
PS:linux BSP 4.1.15

标签 (3)
0 项奖励
回复
1 解答
2,312 次查看
quenreyn
Contributor III

Do you boot with a device tree ? How is set the SD-card node ?

You can add 'disable-wp;' to the node to allow writing accesses.

在原帖中查看解决方案

3 回复数
2,313 次查看
quenreyn
Contributor III

Do you boot with a device tree ? How is set the SD-card node ?

You can add 'disable-wp;' to the node to allow writing accesses.

2,312 次查看
jingyangxie
Contributor V

Hi,Quentin

      thanks for your advice, I will try it

0 项奖励
回复
2,312 次查看
jingyangxie
Contributor V

By the way,the MicroSD can be written and read in Win 10 By adapter,and without adapter in linux 4.1.1.5,It's can only be read

0 项奖励
回复