How to remove the SD card read-only mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to remove the SD card read-only mode

ソリューションへジャンプ
2,489件の閲覧回数
jingyangxie
Contributor V

Hi,all

      I have an imx6q motherboard, when using MicroSD card, the linux always prompts SD card for read-only mode, how can I solve this problem?
PS:linux BSP 4.1.15

ラベル(3)
0 件の賞賛
返信
1 解決策
2,310件の閲覧回数
quenreyn
Contributor III

Do you boot with a device tree ? How is set the SD-card node ?

You can add 'disable-wp;' to the node to allow writing accesses.

元の投稿で解決策を見る

3 返答(返信)
2,311件の閲覧回数
quenreyn
Contributor III

Do you boot with a device tree ? How is set the SD-card node ?

You can add 'disable-wp;' to the node to allow writing accesses.

2,310件の閲覧回数
jingyangxie
Contributor V

Hi,Quentin

      thanks for your advice, I will try it

0 件の賞賛
返信
2,310件の閲覧回数
jingyangxie
Contributor V

By the way,the MicroSD can be written and read in Win 10 By adapter,and without adapter in linux 4.1.1.5,It's can only be read

0 件の賞賛
返信