How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

664 Views
eslam
Contributor I

Hi, 

 

i am using "i.MX 8M Plus EVK Board", and i have flashed on it "LF_v6.12.34-2.1.0_images_IMX8MPEVK" Linux image.

i have made a C++ application on the board which will display some data on an .HTML file

 

So i was asking, is it possible to display data on an .html file on the "i.MX 8M Plus EVK Board"?

does the "i.MX 8M Plus EVK Board" support any kind of web browser?

 

i need to display the data on a GUI on the board itself. 

so please recommend.

 

thanks.

Eslam

0 Kudos
Reply
6 Replies

621 Views
eslam
Contributor I

Hello @JorgeCas

thanks for your answer. 

i have a small question, does this section "5.6.5 Chromium Browser on Wayland" can be applied on the image itself that i have flashed on the board here " L6.12.34-2.1.0_IMX8MP " , or i need to use the source code? if the source code to be used please provide me with the link. 

 

thanks

Eslam 

0 Kudos
Reply

596 Views
JorgeCas
NXP TechSupport
NXP TechSupport
Hello,
You need to build the image to integrate it.
Best regards.
0 Kudos
Reply

522 Views
eslam
Contributor I

Hi @JorgeCas

 

where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks

Tags (1)
0 Kudos
Reply

440 Views
eslam
Contributor I
Hi @JorgeCas

still not get any reply from you here. 

please i need to know where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks.
BR
0 Kudos
Reply

416 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can find it in the next link:

https://github.com/nxp-imx/linux-imx

Best regards.

0 Kudos
Reply

636 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can consider to use Chromium.

The integration can be found in 5.6.5 Chromium Browser on Wayland of i.MX Yocto Project User's Guide.

Best regards.

0 Kudos
Reply