How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

650 次查看
eslam
Contributor I

Hi, 

 

i am using "i.MX 8M Plus EVK Board", and i have flashed on it "LF_v6.12.34-2.1.0_images_IMX8MPEVK" Linux image.

i have made a C++ application on the board which will display some data on an .HTML file

 

So i was asking, is it possible to display data on an .html file on the "i.MX 8M Plus EVK Board"?

does the "i.MX 8M Plus EVK Board" support any kind of web browser?

 

i need to display the data on a GUI on the board itself. 

so please recommend.

 

thanks.

Eslam

0 项奖励
回复
6 回复数

607 次查看
eslam
Contributor I

Hello @JorgeCas

thanks for your answer. 

i have a small question, does this section "5.6.5 Chromium Browser on Wayland" can be applied on the image itself that i have flashed on the board here " L6.12.34-2.1.0_IMX8MP " , or i need to use the source code? if the source code to be used please provide me with the link. 

 

thanks

Eslam 

0 项奖励
回复

582 次查看
JorgeCas
NXP TechSupport
NXP TechSupport
Hello,
You need to build the image to integrate it.
Best regards.
0 项奖励
回复

508 次查看
eslam
Contributor I

Hi @JorgeCas

 

where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks

标记 (1)
0 项奖励
回复

426 次查看
eslam
Contributor I
Hi @JorgeCas

still not get any reply from you here. 

please i need to know where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks.
BR
0 项奖励
回复

402 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can find it in the next link:

https://github.com/nxp-imx/linux-imx

Best regards.

0 项奖励
回复

622 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can consider to use Chromium.

The integration can be found in 5.6.5 Chromium Browser on Wayland of i.MX Yocto Project User's Guide.

Best regards.

0 项奖励
回复