How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to open an .html file in a web browser on the "i.MX 8M Plus EVK Board"

660件の閲覧回数
eslam
Contributor I

Hi, 

 

i am using "i.MX 8M Plus EVK Board", and i have flashed on it "LF_v6.12.34-2.1.0_images_IMX8MPEVK" Linux image.

i have made a C++ application on the board which will display some data on an .HTML file

 

So i was asking, is it possible to display data on an .html file on the "i.MX 8M Plus EVK Board"?

does the "i.MX 8M Plus EVK Board" support any kind of web browser?

 

i need to display the data on a GUI on the board itself. 

so please recommend.

 

thanks.

Eslam

0 件の賞賛
返信
6 返答(返信)

617件の閲覧回数
eslam
Contributor I

Hello @JorgeCas

thanks for your answer. 

i have a small question, does this section "5.6.5 Chromium Browser on Wayland" can be applied on the image itself that i have flashed on the board here " L6.12.34-2.1.0_IMX8MP " , or i need to use the source code? if the source code to be used please provide me with the link. 

 

thanks

Eslam 

0 件の賞賛
返信

592件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport
Hello,
You need to build the image to integrate it.
Best regards.
0 件の賞賛
返信

518件の閲覧回数
eslam
Contributor I

Hi @JorgeCas

 

where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks

タグ(1)
0 件の賞賛
返信

436件の閲覧回数
eslam
Contributor I
Hi @JorgeCas

still not get any reply from you here. 

please i need to know where could i find the correct source code for the image LF_v6.12.34-2.1.0_images_IMX8MPEVK?

thanks.
BR
0 件の賞賛
返信

412件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can find it in the next link:

https://github.com/nxp-imx/linux-imx

Best regards.

0 件の賞賛
返信

632件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You can consider to use Chromium.

The integration can be found in 5.6.5 Chromium Browser on Wayland of i.MX Yocto Project User's Guide.

Best regards.

0 件の賞賛
返信