How to flash Linux BSP Image into SD Card on Windows Machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash Linux BSP Image into SD Card on Windows Machine

ソリューションへジャンプ
7,817件の閲覧回数
nikhil29
Contributor III

Hello NXPTechSupport

 

I'm working on i.MX 8M Mini EVK.

1] How to flash Linux BSP Image into SD Card usind dd command on Windows Machine  [ I don't want to use uuu utility ].

Please help as soon as possible.

 

Regards

Nikhil

0 件の賞賛
返信
1 解決策
7,787件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter 4.3.2 Copying the full SD card image of enclosed file

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
7,788件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the chapter 4.3.2 Copying the full SD card image of enclosed file

 

0 件の賞賛
返信
7,785件の閲覧回数
nikhil29
Contributor III

Thanks joanxie

 

Regards

Nikhil

0 件の賞賛
返信