no output from PMIC imx8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no output from PMIC imx8

963 Views
nadavah
Contributor I

when i check the NVCC_SNVS_1V8 and the VDD_SNVS_0V8 without the imx8 main i see the voltage

but when i put the main back i see no voltage on the outputs and the imx8 dont power up .

any idea what can go wrong ?

im working with bootmode 10 

JTAG-->1

TEST-->0

0 Kudos
Reply
1 Reply

951 Views
igorpadykov
NXP Employee
NXP Employee

Hi nadavah

 

one can recheck power connections using sect.7.11.1 i.MX8 QM/QXP power distribution block diagram

sect.7.12 VDD_MAIN Routing Guidance (i.MX8 QM), clocks in Table 14 – Oscillator/Crystal  Recommendations

i.MX 8QuadMax/i.MX 8QuadXPlus Hardware Developer’s Guide

Schematic for MCIMX8QM-CPU

 

Best regards
igor

0 Kudos
Reply