How to enable yocto uboot MMU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enable yocto uboot MMU?

跳至解决方案
4,093 次查看
wallyyeh
Contributor V

Hi, all:

   our product is based on SDK_3.0.35, recently I'm trying update the uboot and kernel to SDK_3.0.17(yocto build).

    for uboot in SDK_3.0.35, there is one post help people turn on MMU support to speed up uboot:

Linux Fast Boot on i.MX6 Sabresd Board

    but when I move to uboot in SDK_3.10.17(yocto version v2014.01-r0), there is no "board_mmu_init( )" uboot_src/board/freescale/mx6sabresd/mx6sabresd.c.

can some one give me some instruction how to turn on MMU for uboot on SDK_3.10.17? I'll appreciate any kind of helps.


Wally

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
3,236 次查看
fabio_estevam
NXP Employee
NXP Employee

You don't need to do this is in the board file like in the old FSL 2009.08 U-boot. Common code will do this for you.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,237 次查看
fabio_estevam
NXP Employee
NXP Employee

You don't need to do this is in the board file like in the old FSL 2009.08 U-boot. Common code will do this for you.

0 项奖励
回复
3,236 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wally

I think you can look at ..arch/arm/lib/cache-cp15.c

Best regards

chip

0 项奖励
回复