PMU_REG_2P5[ENABLE_WEAK_LINREG] bit in i.MX6SDL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMU_REG_2P5[ENABLE_WEAK_LINREG] bit in i.MX6SDL.

ソリューションへジャンプ
2,335件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to "51.3.2.1 Low Power Operation" in IMX6SDLRM(Rev.1).

There is description of "PMU_REG_2P5[ENABLE_WEAK_LINREG] bit".

But, I couldn't find this register.

On the one hand, I found this register in "50.7 PMU Memory Map/Register Definition" of IMX6DQRM(Rev.2).

[Question]

Why does not the "PMU_REG_2P5[ENABLE_WEAK_LINREG] bit" exist?

Does this bit exist?

Best regards,

Keita

ラベル(2)
0 件の賞賛
返信
1 解決策
2,199件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, exists please refer to attached

rev.2 Manual which soon wil be released.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,200件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, exists please refer to attached

rev.2 Manual which soon wil be released.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,199件の閲覧回数
keitanagashima
Senior Contributor I

Dear chip,

Thank you for your prompt reply.

OK. I got it.

Best Regards,

Keita

0 件の賞賛
返信