How to enable yocto uboot MMU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable yocto uboot MMU?

Jump to solution
4,042 Views
wallyyeh
Contributor V

Hi, all:

   our product is based on SDK_3.0.35, recently I'm trying update the uboot and kernel to SDK_3.0.17(yocto build).

    for uboot in SDK_3.0.35, there is one post help people turn on MMU support to speed up uboot:

Linux Fast Boot on i.MX6 Sabresd Board

    but when I move to uboot in SDK_3.10.17(yocto version v2014.01-r0), there is no "board_mmu_init( )" uboot_src/board/freescale/mx6sabresd/mx6sabresd.c.

can some one give me some instruction how to turn on MMU for uboot on SDK_3.10.17? I'll appreciate any kind of helps.


Wally

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
3,185 Views
fabio_estevam
NXP Employee
NXP Employee

You don't need to do this is in the board file like in the old FSL 2009.08 U-boot. Common code will do this for you.

View solution in original post

0 Kudos
Reply
2 Replies
3,186 Views
fabio_estevam
NXP Employee
NXP Employee

You don't need to do this is in the board file like in the old FSL 2009.08 U-boot. Common code will do this for you.

0 Kudos
Reply
3,185 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wally

I think you can look at ..arch/arm/lib/cache-cp15.c

Best regards

chip

0 Kudos
Reply