How to enable native and gpio cs on ecspi

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable native and gpio cs on ecspi

5,672 次查看
alimalik
Contributor II

Hi

I am having some issue getting the SPI to work on IMX6. The question I have is how do we enable multiple CS on SPI. This is what I currently have.

ecspi1 is using its 2 native chipselects and I also have a gpio CS.

This is what i did in my .dtsi file

ecspi1 {

        pinctrl_ecspi1_cs_1: ecspi1_cs_grp-1 {

            fsl,pins = <

                MX6QDL_PAD_KEY_ROW2__GPIO4_IO11 0x80000000 /* GPIO CS*/

                MX6QDL_PAD_KEY_COL2__ECSPI1_SS1 0x80000000

                MX6QDL_PAD_KEY_ROW1__ECSPI1_SS0 0x80000000

            >;

        };

&ecspi1 {

    fsl,spi-num-chipselects = <3>;

    cs-gpios = <&gpio4 11 0>, <&gpio4 10 0>, <&gpio4 9 0>;

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_ecspi1_2>, <&pinctrl_ecspi1_cs_1>;

    status = "okay";

    ads7846@0x00 {

        reg = <0>;    /* CS0 */

        compatible = "ti,ads7846";

        interrupt-parent = <&gpio1>;

        interrupts = <4 1>;   

        spi-max-frequency = <1500000>;

        pendown-gpio = <&gpio1 4 0>;

        vcc-supply = <&reg_soc>;

        ti,x-min = /bits/ 16 <4200>;

        ti,x-max = /bits/ 16 <8080>;

        ti,y-min = /bits/ 16 <4330>;

        ti,y-max = /bits/ 16 <7980>;

        ti,x-plate-ohms = /bits/ 16 <180>;

        ti,pressure-max = /bits/ 16 <255>;

        ti,debounce-max    = /bits/ 16 <10>;

        ti,debounce-tol = /bits/ 16 <3>;

        ti,debounce-rep    = /bits/ 16 <1>;

        ti,settle-delay-usec    = /bits/ 16 <150>;

        ti,keep-vref-on;

        ti,swap-xy;   

        linux,wakeup;

    };

   

    io_expander_1: spi_imx@0x00 {

        compatible = "spi_imx";

        spi-max-frequency = <20000000>;

        reg = <1>;

    };

    io_expander_2: spi_imx@0x01 {

        compatible = "spi_imx";

        spi-max-frequency = <20000000>;

        reg = <2>;

    };

};

But I dont seem to get the io_expanders enables and noting appears in my /dev folder.

Any Ideas

0 项奖励
回复
2 回复数

3,900 次查看
yann_cardaillac
Contributor II

Hi there,

Well sorry to dug this pretty old post, but here what one should have done to use several cs.

&ecspi1 {

    fsl,spi-num-chipselects = <3>;

    cs-gpios = <&gpio4 11 0>, <&gpio4 10 0>, <&gpio4 9 0>;

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_ecspi1_2>, <&pinctrl_ecspi1_cs_1>;

    status = "okay";

 

    ads7846@0x00 {

        reg = <0>;    /* CS0 */

        ...

    };

   

    io_expander_1: spi_imx@0x01 {

        ...

        reg = <1>;

    };

 

    io_expander_2: spi_imx@0x02 {

        ...

        reg = <2>;

    };

};

Regards,

0 项奖励
回复

3,900 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

According to this: https://www.kernel.org/doc/Documentation/devicetree/bindings/spi/spi-bus.txt

you may try something like the next example in the cs-gpios property.

cs-gpios = <&gpio1 0 0> <0> <&gpio1 1 0> <&gpio1 2 0>;

Then it should be configured so that num_chipselect = 4 with the

following mapping:

cs0 : &gpio1 0 0

cs1 : native

cs2 : &gpio1 1 0

cs3 : &gpio1 2 0

I hope that helps,

Alejandro