imx6q android P can't boot after fastboot oem unlock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q android P can't boot after fastboot oem unlock

2,513件の閲覧回数
fdact
Contributor I

Hi,
   My boarid is imx6q and works on Android P9.0.0_2.2.0 (4.14.98 kernel).
The compiled version of android P is userdebug. It tells me that the "device is locked" when I use
"adb remount". when I do follow the steps, the android P can't boot:
    1.go to setting -> system -> Developer options -> OEM unlocking
    2.adb reboot bootloader
    3.fastboot oem unlock
    4.fastboot reboot

the log stop here,and system is not running:

zram0: detected capacity change from 0 to 536870912
logd.auditd: start
mkswap: Swapspace size: 524284k, UUID=3702fdde-cd96-4fe0-872c-3a98fb38ee5e
Adding 524284k swap on /dev/block/zram0.  Priority:-2 extents:1 across:524284k SS
random: crng init done

Attached is the complete log.

Thanks.

ラベル(3)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,320件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you able to see your device in fast boot mode with ./fastboot.exe devices?

Best regards,

Diego.

0 件の賞賛
返信

2,319件の閲覧回数
shivanipatel
Senior Contributor II

Hi, zero zero 

We have built the Android 9 by following the steps given in the attached Android User Guide. I am able to reboot the board with fastboot reboot command.

Let us know if you are facing the issue with these steps.

Regards,

Shivani

0 件の賞賛
返信

2,319件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Let me try to reproduce your problem. Since you are doing the steps in the right way.

Best regards,

Diego.

0 件の賞賛
返信