How to enable can bus on i.MX6 SabreAI ported with Androidkk4.4.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable can bus on i.MX6 SabreAI ported with Androidkk4.4.3

1,772 Views
bandelaprathyus
Contributor II

Hi,

    We have Flex can support in android. 

->busybox ifconfig -a have can0 in the list.

-> The command ip link set can0 up type can bitrate 125000 is starting the can0 interface, I have verified that by giving "netcfg".

->But it does not support canutils,cantest.

->What is the procedure to be followed to have can bus support in android.

->I am using Sabre i.mx6 Sabre Ai Board with Android KK4.3.2

Labels (2)
0 Kudos
Reply
1 Reply

1,326 Views
igorpadykov
NXP Employee
NXP Employee

Hi bandela

please check below links where such support is described

How to use FlexCAN in Android OS

6 CANbus PhyCORE-AM335X Jelly Bean Android Development - PHYTEC Wiki

Controller Area Network (CAN) support in Android LibBits | Little bits of information on everything

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply