PCIe endpoint driver with DMA support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe endpoint driver with DMA support

2,951件の閲覧回数
shabbirlimdiwal
Contributor I

Hi,

Is i.mx6 quad validated with PCIe end point mode in Linux? Is DMA implementation already available for PCIe end point?

We have a high throughput requirement (output 720P30, YUV422) over PCIe. Will i.mx6 quad be sufficient enough to do so?

Thanks and Regards,

Shabbir

タグ(2)
0 件の賞賛
返信
1 返信

2,220件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shabbir

yes it is validated

i.MX6Q PCIe EP/RC Validation System

please also check attached document sect.35.5 i.MX 6Quad SD PCIe RC/EP Validation System

included in L3.0.35_4.1.0_ER_SOURCE_BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信