How to enable QSPI_B in imx8m?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable QSPI_B in imx8m?

2,521 次查看
prajna_nayak
Contributor I

Hi,

I'm using imx8m custom board, linux 4.9.51 ga release.

I'm trying to implement QSPI_A and QSPI_B in imx8m platform. I'm able to add QSPI_A(alone) successfully. If I add both QSPI_A and B, the board hangs. If I try to add QSPI_B alone by disabling A, I get the below messages:

=======================================================

# dmesg | grep -i spi                                                                                                                                    
 fsl-quadspi 30bb0000.qspi: unrecognized JEDEC id bytes: 00, 00, 00
 fsl-quadspi 30bb0000.qspi: Freescale QuadSPI probe failed
 fsl-quadspi: probe of 30bb0000.qspi failed with error -2

========================================================

Following is the dts node and pin controls I'm using.

&qspi {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_qspi>;
        status = "okay";

        flash0: mt25qu256aba@0 {
                reg = <0>;
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "micron,mt25qu256aba";
                spi-tx-bus-width = <4>;
                spi-rx-bus-width = <4>;
                spi-max-frequency = <12000000>;
                spi-nor,ddr-quad-read-dummy = <6>;
                status="okay";
        };

      flash1: mt25qu256aba@1 {
                reg = <1>;
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "micron,mt25qu256aba";
                spi-tx-bus-width = <4>;
                spi-rx-bus-width = <4>;
                spi-max-frequency = <12000000>;
                spi-nor,ddr-quad-read-dummy = <6>;
                status = "okay";
        };
};

....

 pinctrl_qspi: qspigrp {
                        fsl,pins = <
                                MX8MQ_IOMUXC_NAND_ALE_QSPI_A_SCLK       0x82
                                MX8MQ_IOMUXC_NAND_CE0_B_QSPI_A_SS0_B    0x82
                                MX8MQ_IOMUXC_NAND_DATA00_QSPI_A_DATA0   0x82
                                MX8MQ_IOMUXC_NAND_DATA01_QSPI_A_DATA1   0x82
                                MX8MQ_IOMUXC_NAND_DATA02_QSPI_A_DATA2   0x82
                                MX8MQ_IOMUXC_NAND_DATA03_QSPI_A_DATA3   0x82

                                MX8MQ_IOMUXC_NAND_CLE_QSPI_B_SCLK       0x82
                                MX8MQ_IOMUXC_NAND_DATA04_QSPI_B_DATA0   0x82
                                MX8MQ_IOMUXC_NAND_DATA05_QSPI_B_DATA1   0x82
                                MX8MQ_IOMUXC_NAND_CE2_B_QSPI_B_SS0_B    0x82
                                MX8MQ_IOMUXC_NAND_DATA06_QSPI_B_DATA2   0x82
                                MX8MQ_IOMUXC_NAND_DATA07_QSPI_B_DATA3   0x82
                        >;
                };

Is this correct? There is no clock when I probe. Is there anything which is needed to be added to enable QSPI_B apart from the dts?

Thanks in advance.

Regards,

Prajna

标记 (2)
0 项奖励
回复
3 回复数

2,005 次查看
jimmychan
NXP TechSupport
NXP TechSupport

please check the chapter 10.2.3.4. There are the Memory Map of Flash A and B in the i.MX8M RM.

0 项奖励
回复

2,005 次查看
prajna_nayak
Contributor I

Hi Jimmychan,

Thanks for the reply. Is there any change to be done in dts or driver file? If yes, what are the changes?

Regards,

Prajna

0 项奖励
回复

2,005 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Did you use symmetric NOR chips?

for example:

 

pastedImage_1.png

If two chips(or two planes in one die) are symmetric, the driver should work fine, please follow the i.MX6SX dtb settings below:

 

&qspi1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_qspi1_1>;
status = "okay";
ddrsmp=<2>;

flash0: n25q256a@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "micron,n25q256a";
spi-max-frequency = <29000000>;
reg = <0>;
};

flash1: n25q256a@1 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "micron,n25q256a";
spi-max-frequency = <29000000>;
reg = <1>;
};

};

0 项奖励
回复