i.MX6Q DQS gating calibration question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q DQS gating calibration question

905 Views
Danube
Contributor IV

Hi All,

We alrways use DDR calibration tool to get some value.

But why Final Value is "End-0.5*tCK:" not "Mean" ?

Example

BYTE 0:

    Start:         HC=0x01 ABS=0x1C

    End:         HC=0x04 ABS=0x5C

    Mean:         HC=0x02 ABS=0x7B

    End-0.5*tCK:     HC=0x03 ABS=0x5C

    Final:         HC=0x03 ABS=0x5C

BYTE 1:

    Start:         HC=0x02 ABS=0x18

    End:         HC=0x04 ABS=0x4C

    Mean:         HC=0x03 ABS=0x32

    End-0.5*tCK:     HC=0x03 ABS=0x4C

    Final:         HC=0x03 ABS=0x4C

DQS calibration MMDC0 MPDGCTRL0 = 0x034C035C, MPDGCTRL1 = 0x03480340

DQS calibration MMDC1 MPDGCTRL0 = 0x03680370, MPDGCTRL1 = 0x035C0324

0 Kudos
1 Reply

751 Views
igorpadykov
NXP Employee
NXP Employee

Hi Appolo

reason may be that using algorithm described in Figure 9. DQS Read Gating

Calibration: Timing Diagram AN4467 i.MX 6 Series DDR Calibration, difference between

too-early and too-late gate boundaries is one equal cycle, so when exceeding it

program considers more reliable to use too-late gate boundary and subtract 0.5tCK.

https://www.nxp.com/docs/en/application-note/AN4467.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos