How to debug u-boot.imx by SD Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to debug u-boot.imx by SD Card

跳至解决方案
1,983 次查看
road_wang
Contributor I

             My I.MX6UL system is running on SD Card,when I modify some codes on U-Boot code and generated new u-boot.imx,for cann't find u-boot.imx on the SD Card,how to update u-boot.imx on SD Card for debug.

0 项奖励
回复
1 解答
1,915 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,915 次查看
road_wang
Contributor I

but there isn't u-boot.imx on sdcard,I can't copy it to sdcard directly. How can update u-boot.imx on sdcard?

0 项奖励
回复
1,916 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

0 项奖励
回复
1,915 次查看
road_wang
Contributor I

Hi Rita,

 Because my board nand flash size is only 256M,but the image build from Yocto project is larger than it,So I only use sdcard to debug now. Can update u-boot on SDCard?

Best Regards

Road

0 项奖励
回复
1,915 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, if your board support sdcard, you can use it.

0 项奖励
回复