How to debug u-boot.imx by SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug u-boot.imx by SD Card

Jump to solution
1,975 Views
road_wang
Contributor I

             My I.MX6UL system is running on SD Card,when I modify some codes on U-Boot code and generated new u-boot.imx,for cann't find u-boot.imx on the SD Card,how to update u-boot.imx on SD Card for debug.

0 Kudos
Reply
1 Solution
1,907 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

View solution in original post

0 Kudos
Reply
4 Replies
1,907 Views
road_wang
Contributor I

but there isn't u-boot.imx on sdcard,I can't copy it to sdcard directly. How can update u-boot.imx on sdcard?

0 Kudos
Reply
1,908 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Wang,

If you modify the u-boot you need to download the new one to your board. You can use the mfgtool to download. If you are using the newest BSP you need to use the tool UUU.

Hope this can do help for you

Have a nice day

Best Regards

Rita

0 Kudos
Reply
1,907 Views
road_wang
Contributor I

Hi Rita,

 Because my board nand flash size is only 256M,but the image build from Yocto project is larger than it,So I only use sdcard to debug now. Can update u-boot on SDCard?

Best Regards

Road

0 Kudos
Reply
1,907 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, if your board support sdcard, you can use it.

0 Kudos
Reply