How to correctly set CONFIG_SYS_LDB_CLOCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to correctly set CONFIG_SYS_LDB_CLOCK

跳至解决方案
1,401 次查看
marcosal
Contributor II

Hi, sorry if the question is dummy, I started to work on embedded systems some weeks ago =).

I'm working with an IMX6 Dual .

I would like to know how to set the correct value for the define "#define CONFIG_SYS_LDB_CLOCK 65000000" in the file ipu_common.c in the spl.

the settings for the display are (in both spl setup file and ldb.c kernel file):

struct fb_videomode mode_display= {
.name = "1920x720",
.refresh = 60,
.xres = 1920,
.yres = 720,

/*
LVDS-Clock:
 1 / (48,7MHz * 2)
 10267
*/
.pixclock = 10267,
.left_margin = 40,
.right_margin = 48,
.upper_margin = 2,
.lower_margin = 3,
.hsync_len = 40,
.vsync_len = 4,
.sync = FB_SYNC_EXT,
.vmode = FB_VMODE_NONINTERLACED
};

The setup_display (spl) performs the following operations (I use smooth transition since I'm displaying a splash screen):

void setup_display(void)
{
    struct mxc_ccm_reg *mxc_ccm = (struct mxc_ccm_reg *)CCM_BASE_ADDR;

    reg = readl(&mxc_ccm->CCGR3);
    reg |= MXC_CCM_CCGR3_IPU2_IPU_MASK;
    writel(reg, &mxc_ccm->CCGR3);

    reg = readl(&mxc_ccm->CCGR3);
    reg &= ~MXC_CCM_CCGR3_LDB_DI1_MASK;
    reg |= MXC_CCM_CCGR3_LDB_DI0_MASK;
    writel(reg, &mxc_ccm->CCGR3);

#ifdef MAN_IMX_SPREAD_SPRECTRUM_ENABLED

    reg = readl(&mxc_ccm->analog_pfd_528);
    reg &= ~(BM_ANADIG_PFD_528_PFD2_FRAC);
    reg |= BF_ANADIG_PFD_528_PFD2_FRAC(0x1C);
    writel(reg, &mxc_ccm->analog_pfd_528);

    /* Spread spectrum numerator */
    reg =BF_ANADIG_PLL_528_DENOM_B(MAN_SPREAD_SPECTRUM_DENOM_B);
    writel(reg, &mxc_ccm->analog_pll_528_denom);

    reg = readl(&mxc_ccm->analog_pll_528_ss);
    reg |= BF_ANADIG_PLL_528_SS_STEP(MAN_SPREAD_SPECTRUM_STEP);
    reg |= BF_ANADIG_PLL_528_SS_STOP(MAN_SPREAD_SPECTRUM_STOP);
    reg |= BM_ANADIG_PLL_528_SS_ENABLE; /* Enable Spread Spectrum*/
    writel(reg, &mxc_ccm->analog_pll_528_ss);

    reg = readl(&mxc_ccm->cs2cdr);
    // Select PLL2 for ldb_diX_clk_sel
    reg &= ~(MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_MASK);
    reg |= (MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_PLL2_396M_PFD <<     MXC_CCM_CS2CDR_LDB_DI0_CLK_SEL_OFFSET);
    writel(reg, &mxc_ccm->cs2cdr);
#else

    .... // code doesn't enter here

#endif

    //Divider for 3.5
    reg = readl(&mxc_ccm->cscmr2);
    reg &= ~(MXC_CCM_CSCMR2_LDB_DI0_IPU_DIV);
    writel(reg, &mxc_ccm->cscmr2);

    //Clocks for IPU2
    reg = readl(&mxc_ccm->cscdr2);

    /* Use ipu2 root clock from LDB_DI0 */
    reg &= ~(MXC_CCM_CHSCCDR_IPU2_DI0_CLK_SEL_MASK);
    reg |= (CHSCCDR_CLK_SEL_LDB_DI0 << MXC_CCM_CHSCCDR_IPU2_DI0_CLK_SEL_OFFSET);
    writel(reg, &mxc_ccm->cscdr2);

}

the ipu_common.c has:

#if !defined CONFIG_SYS_LDB_CLOCK
#define CONFIG_SYS_LDB_CLOCK 65000000
#endif

static struct clk ldb_clk = {
.name = "ldb_clk",
.rate = CONFIG_SYS_LDB_CLOCK,
.usecount = 0,
};

Thanks for any solution or advise.

0 项奖励
回复
1 解答
1,197 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Marcos

one can look at below examples for configuring ldb clocks

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,198 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Marcos

one can look at below examples for configuring ldb clocks

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------