How to convert wbf waveform file to wf file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to convert wbf waveform file to wf file?

10,694件の閲覧回数
ningli
Contributor III

Hi,

i am using imx6sololite evk board in my project.Now i got a waveform file *.wbf, but bsp code using wf file.

Is there any method to covert this file format?

Original Attachment has been moved to: 320_G087_AB0203_ED060XG3T1_TC-NG.wbf.zip

ラベル(4)
0 件の賞賛
返信
20 返答(返信)

9,891件の閲覧回数
ningli
Contributor III

thanks! is there any patch to support wbf format?

0 件の賞賛
返信

9,890件の閲覧回数
yan2anfei
Contributor III

hi Artur,

    my *.wbf file is in the attachment. thanks!

Best Regards,

yan2anfei

0 件の賞賛
返信

9,890件の閲覧回数
art
NXP Employee
NXP Employee

Please find attached the converted .fw file for the i.MX7Dual processor's EPD controller.


Have a great day,
Artur

9,890件の閲覧回数
yan2anfei
Contributor III

hi Artur,

my *.wbf waveform support the GLR16 GLD16 mode. 

Is the *.fw file which you help me  convet  suppurt "REGAL/-D"  feature?

 

thanks && best reagrds.

yan2anfei

0 件の賞賛
返信

9,890件の閲覧回数
art
NXP Employee
NXP Employee

Yes, it supports.

Best Regards,

Artur

0 件の賞賛
返信

9,886件の閲覧回数
进林桂
Contributor I

hi Artur,

 Could you help me covert the wbf file to fw file for i.MX6SL, wbf is attached.

 thanks. 

0 件の賞賛
返信

9,890件の閲覧回数
yan2anfei
Contributor III

Dear Artur,

Could you help me converted the *.fw file to *_splash.bin ,I need to display a picture in my u-boot screen.

the *.fw file is which you  has help me converted. 

Thandks&Best Regards

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

Refer to the Section 10.3.7 "Enabling an EPDC Splash Screen" of the attached document. The required python script is also attached.

Artur

9,878件の閲覧回数
yan2anfei
Contributor III

hi Artur,

I my tools convert *.wbf to *.fw can't works well,

can you help me convert a waveform for imx6sl,the *.wbf is attached.

thanks && best reagrds.

yan2anfei

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

Please find attached.

Best Regards,

Artur

0 件の賞賛
返信

9,878件の閲覧回数
yan2anfei
Contributor III

dear Artur,

the 320_R137_TC1.fw is 5bit waveform,  It  can't work .

the older  waveform SCM060.fw can work which is 4bit format.

Is the imx6sl platform can't support my e-ink display screen. or the sourcecode need to Modify.

thanks & bestregards,

yan2anfei

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

After further studying the case, I've found the following. As per the i.MX6SoloLite Reference Manual document, its EPD Controller hardware itself supports the 5-bit pixel format. However, the current framebuffer driver seems to be supporting only 4-bit format. So, only 4-bit EP displays can be supported in Linux at present.

Artur

0 件の賞賛
返信

9,878件の閲覧回数
yan2anfei
Contributor III

thanks very much 

Best Regards

yan2anfei

0 件の賞賛
返信

9,878件の閲覧回数
yan2anfei
Contributor III

It works well,thanks very much!

Best Regards,

yan2anfei

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

No, the BSPs support only the .fw format.

Artur

9,878件の閲覧回数
art
NXP Employee
NXP Employee

Please find attached the resulting .fw file.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

9,878件の閲覧回数
yan2anfei
Contributor III

hi Artur,

     I am using imx7dsabre evk board in my project.Now I got a waveform file *.wbf, but bsp code using wf file.  Could you help me covert the file .

 thanks. 

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

Send me your .wbf file and I will convert it to .fw.

Best Regards,

Artur

0 件の賞賛
返信

9,878件の閲覧回数
ningli
Contributor III

Hi ,

when i decompression 320_G087_AB0203_ED060XG3T1_TC-NG.fw.zip, I got a file 320_G087_AB0203_ED060XG3T1_TC-NG.fw but the file size is 4.75MB. Is it right? because original file size is 234KB.

0 件の賞賛
返信

9,878件の閲覧回数
art
NXP Employee
NXP Employee

Yes, this is right. The reason is that the .wbf file contains the symbolic description of a EPD control waveforms, whereas the .fw file contains the representation of a waveforms in binary format, that is much more larger than the symbolic one.

Artur

0 件の賞賛
返信