How can ı use gstream with OpenCV

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can ı use gstream with OpenCV

6,407 Views
yaşarcani_tişge
Contributor II

Hi,

I am using İ.MXQ6sabresd development board. I want to use gstreamer with Opencv. I want to capturing and processing video frames with OpenCV .  But my code did not work.How can ı do it ? My code:

#include "opencv2/objdetect/objdetect.hpp"
#include "opencv2/highgui/highgui.hpp"
#include "opencv2/imgproc/imgproc.hpp"
#include <iostream>
#include <stdlib.h>


using namespace std;
using namespace cv;

String window_name = "Face Detection";

void detectFaces(Mat frame, int frameno) {

CascadeClassifier face_cascade;
face_cascade.load("/usr/examples/facevide/haarcascade_frontalface_alt.xml");
CascadeClassifier eye_cascade;
eye_cascade.load("/usr/examples/facevide/haarcascade_eye.xml");
std::vector<Rect> faces;

face_cascade.detectMultiScale( frame, faces, 1.1, 2, 0|CV_HAAR_SCALE_IMAGE,
Size(30, 30) );
std::vector<Rect> eyes;
eye_cascade.detectMultiScale( frame, eyes, 1.1, 2, 0 |CV_HAAR_SCALE_IMAGE,
Size(100, 100) );
std::ostringstream name;
name << "rotated_im_" << frameno << ".jpg";
for( int i = 0; i < faces.size(); i++ ){
Point center(faces[i].x + faces[i].width/2, faces[i].y + faces[i].height/2);
ellipse(frame, center, Size(faces[i].width/2, faces[i].height/2), 0, 0, 360, Scalar( 255, 0,
255 ), 4, 8, 0 );
for( int j = 0; j < eyes.size(); j++ )
 {
Point eyes_center( eyes[j].x + eyes[j].width/2, eyes[j].y + eyes[j].height/2 );
int radius = cvRound( (eyes[j].width + eyes[j].height)*0.25 );
circle( frame, eyes_center, radius, Scalar( 255, 0, 0 ), 4, 8, 0 );
}
}
imwrite(name.str(), frame); // Display frame
}
int main() {
//VideoCapture cap("gst-launch-1.0 imxv4l2src ! autovideosink ! appsink");
VideoCapture cap("gst-launch-1.0 autovideosrc ! autovideosink");
//VideoCapture cap(" mfw_v4lsrc ! ffmpegcolorspace ! video/x-raw-rgb ! appsink");
//VideoCapture cap("v4l2src ! video/x-raw, framerate=30/1, width=640, height=480, format=RGB ! videoconvert ! appsink");
//const char* pipe =  "rtspsrc location=\"rtsp://192.168.0.220:554/user=admin&password=admin&channel=1&
VideoCapture cap("gst-launch mfw_v4lsrc num-buffers=1 !  jpegenc ! filesink location=sample.jpeg");

Mat frame;
int i = 0;
while(cap.read(frame)) {
detectFaces(frame, i);
i++;
                          }
                     }

Thank you.

Yasarcan

 
Labels (4)
7 Replies

4,162 Views
yaşarcani_tişge
Contributor II
 
I use a camera connected to the board. (Camera: MIPI OV5642)
0 Kudos
Reply

4,162 Views
joanxie
NXP TechSupport
NXP TechSupport

did you use ov5642 or ov5640? ov5640 is mipi, pls comfirm this,

0 Kudos
Reply

4,162 Views
yaşarcani_tişge
Contributor II

I tried them. But it does not work. I made some changes to my code. Not working again. joanxie

    for(;;)
    {
      Mat frame;
      int i = 0;
      printf("for dongusu\n");
   //  while(cap.read(frame)) {
     cap >> frame;
     if (frame.empty()) {
         printf("no frame\n");
         break;
     printf("while dongusu\n");
      deneme(frame, i);
      i++;
    }
  }
}

I tried more than one option but did not work at all

//string gst_pipe = "videotestsrc ! videoconvert ! appsink";
    //VideoCapture cap(gst_pipe);
    //VideoCapture cap( "v4l2src ! filesink location=file.jpg" );
    //VideoCapture cap(" mfw_v4lsrc ! videoconvert ! appsink");
    VideoCapture cap("-v udpsrc port=5000 caps=application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)RAW, sampling=(string)BGR, depth=(string)8, width=(string)640, height=(string)480 ! rtpvrawdepay ! videoconvert ! ximagesink");
     // VideoCapture cap( "VSALPHA=1 gst-launch-1.0 filesrc location=<filename> ! jpegdec ! imagefreeze ! autovideosink" );
    //VideoCapture cap(" mfw_v4lsrc ! mfw_ipucsc ! appsink");
    //VideoCapture cap(" mfw_v4lsrc num-buffers=1 !  jpegenc ! filesink location=sample.jpeg");
    //VideoCapture cap("autovideosrc ! autovideoconvert ! appsink");
    //VideoCapture cap( "autovideosrc ! video/x-raw,format=YUY2 ! videoconvert !appsink" );
    //VideoCapture cap( "v4l2src num-buffers=1 ! ffmpegcolorspace ! video/x-raw-yuv,width=640,height=480,framerate=8/1 ! jpegenc ! filesink location=test.jpg  " );
    //VideoCapture cap("mfw_v4lsrc ! ffmpegcolorspace ! video/x-raw-rgb ! appsink");
    //VideoCapture cap("v4l2src num-buffers=1 ! ffmpegcolorspace ! video/x-raw-yuv,width=640,height=480,framerate=8/1 ! jpegenc ! filesink location=test.jpg ");
    //VideoCapture cap("v4l2src ! jpegdec ! ffmpegcolorspace ! ximagesink");
    //VideoCapture cap("-v imxfslv4l2src device=/dev/video1 ! imxv4l2sink");
    //VideoCapture cap("imxv4l2src num-buffers=1 device=/dev/video1 ! jpegenc ! filesink location=picture.jpg");
    //VideoCapture cap(" imxv4l2src num-buffers=1 device=/dev/video1 ! video/x-raw, format=(string)YUY2, width=(int)2592, height=(int)1944, framerate=15/1 ! jpegenc ! filesink location=test.jpg" );

0 Kudos
Reply

4,162 Views
yaşarcani_tişge
Contributor II

I tried  " VideoCapture cap("autovideosrc !  autovideoconvert ! appsink ");  but it doesn`t work. How else can I turn it ? joanxie

0 Kudos
Reply

4,162 Views
joanxie
NXP TechSupport
NXP TechSupport

you also can try to use

"VideoCapture cap("mfw_v4lsrc ! ffmpegcolorspace ! video/x-raw-rgb ! appsink")" for converting yuv to rgb format
0 Kudos
Reply

4,162 Views
joanxie
NXP TechSupport
NXP TechSupport
do you use webcam? try to use the command as below:
  • gst-launch-1.0 -v udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)RAW, sampling=(string)BGR, depth=(string)8, width=(string)640, height=(string)480" ! rtpvrawdepay ! videoconvert ! ximagesink
0 Kudos
Reply

4,162 Views
joanxie
NXP TechSupport
NXP TechSupport

the camera output is yuv, you should convert to the yuv to pass opencv, try to use rgb format and try again