How to connect camera and IPU-CSI2 port ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect camera and IPU-CSI2 port ?

Jump to solution
1,494 Views
kanoumamoru
Contributor III

Our customer want to use the second camera using IPU2-CSI1 parallel interface.

IPU2-CSI1 pin allocation may be following.

MX6Q_PAD_EIM_A17 <= IPU2_CSI1_D_12,

MX6Q_PAD_EIM_A18 <= IPU2_CSI1_D_13,

MX6Q_PAD_EIM_A19 <= IPU2_CSI1_D_14,

MX6Q_PAD_EIM_A20 <= IPU2_CSI1_D_15,

MX6Q_PAD_EIM_D19 <= IPU2_CSI1_D_16,

MX6Q_PAD_EIM_A22 <= IPU2_CSI1_D_17,

MX6Q_PAD_EIM_A23 <= IPU2_CSI1_D_18,

MX6Q_PAD_EIM_A24 <= IPU2_CSI1_D_19,

According to i.MX6dq data sheet, after out of reset, these pins become the output port and out low level signal.

Therefore, after reset, Do we must not tie a signal of the CMOS camera to EIM_A[17:24] until  MUX_MODE is changed ?


pastedImage_0.png

Best Regards.

kanou

Labels (1)
0 Kudos
Reply
1 Solution
1,254 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

yes your understanding is correct:

due to signal contention it is not recommended

to tie/enable a signal from CMOS camera to EIM_A[17:24] until 

MUX_MODE is changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,255 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

yes your understanding is correct:

due to signal contention it is not recommended

to tie/enable a signal from CMOS camera to EIM_A[17:24] until 

MUX_MODE is changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply