How to connect camera and IPU-CSI2 port ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to connect camera and IPU-CSI2 port ?

跳至解决方案
1,517 次查看
kanoumamoru
Contributor III

Our customer want to use the second camera using IPU2-CSI1 parallel interface.

IPU2-CSI1 pin allocation may be following.

MX6Q_PAD_EIM_A17 <= IPU2_CSI1_D_12,

MX6Q_PAD_EIM_A18 <= IPU2_CSI1_D_13,

MX6Q_PAD_EIM_A19 <= IPU2_CSI1_D_14,

MX6Q_PAD_EIM_A20 <= IPU2_CSI1_D_15,

MX6Q_PAD_EIM_D19 <= IPU2_CSI1_D_16,

MX6Q_PAD_EIM_A22 <= IPU2_CSI1_D_17,

MX6Q_PAD_EIM_A23 <= IPU2_CSI1_D_18,

MX6Q_PAD_EIM_A24 <= IPU2_CSI1_D_19,

According to i.MX6dq data sheet, after out of reset, these pins become the output port and out low level signal.

Therefore, after reset, Do we must not tie a signal of the CMOS camera to EIM_A[17:24] until  MUX_MODE is changed ?


pastedImage_0.png

Best Regards.

kanou

标签 (1)
0 项奖励
回复
1 解答
1,277 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

yes your understanding is correct:

due to signal contention it is not recommended

to tie/enable a signal from CMOS camera to EIM_A[17:24] until 

MUX_MODE is changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,278 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mamoru

yes your understanding is correct:

due to signal contention it is not recommended

to tie/enable a signal from CMOS camera to EIM_A[17:24] until 

MUX_MODE is changed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复