How to change the partition format from MBR to GPT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the partition format from MBR to GPT

跳至解决方案
2,453 次查看
Y_K
Contributor I

Hi,

I want to create more than 4 partitions on emmc of i.MX 8m plus.

I read AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).
"4.2 Partitioning at the image deployment stage" has instructions for changing to mbr.
Q1) Is the default partition format of imx8m series gpt?

I'm currently using the images in LF_v5.15.5-1.0.0_images_iMX8MPEVK, but the partition format is configured as MBR.

Q2) Why is the LF_v5.15.5-1.0.0_images_iMX8MPEVK image configured with MBR? Do you have a reason?

Q3) Is it possible to change from MBR to GPT? Any problems?

Q4) Where should I modify to change from MBR to GPT?

0 项奖励
回复
1 解答
2,409 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,410 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada
0 项奖励
回复
2,380 次查看
Y_K
Contributor I

Hi,  @Dhruvit 

Sorry for the late reply.

I tried reading the document you provided.
Solved without incident.

thank you very much.

0 项奖励
回复
2,363 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Glad to know that issue is resolved.

Can I mark this case as close?

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复
2,358 次查看
Y_K
Contributor I

Hi, @Dhruvit 

>Can I mark this case as close?
   Yes, it is okay.
   thank you very much.

0 项奖励
回复