How to change the partition format from MBR to GPT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the partition format from MBR to GPT

ソリューションへジャンプ
2,358件の閲覧回数
Y_K
Contributor I

Hi,

I want to create more than 4 partitions on emmc of i.MX 8m plus.

I read AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).
"4.2 Partitioning at the image deployment stage" has instructions for changing to mbr.
Q1) Is the default partition format of imx8m series gpt?

I'm currently using the images in LF_v5.15.5-1.0.0_images_iMX8MPEVK, but the partition format is configured as MBR.

Q2) Why is the LF_v5.15.5-1.0.0_images_iMX8MPEVK image configured with MBR? Do you have a reason?

Q3) Is it possible to change from MBR to GPT? Any problems?

Q4) Where should I modify to change from MBR to GPT?

0 件の賞賛
返信
1 解決策
2,314件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,315件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada
0 件の賞賛
返信
2,285件の閲覧回数
Y_K
Contributor I

Hi,  @Dhruvit 

Sorry for the late reply.

I tried reading the document you provided.
Solved without incident.

thank you very much.

0 件の賞賛
返信
2,268件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Glad to know that issue is resolved.

Can I mark this case as close?

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信
2,263件の閲覧回数
Y_K
Contributor I

Hi, @Dhruvit 

>Can I mark this case as close?
   Yes, it is okay.
   thank you very much.

0 件の賞賛
返信