How to change the partition format from MBR to GPT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the partition format from MBR to GPT

Jump to solution
2,431 Views
Y_K
Contributor I

Hi,

I want to create more than 4 partitions on emmc of i.MX 8m plus.

I read AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).
"4.2 Partitioning at the image deployment stage" has instructions for changing to mbr.
Q1) Is the default partition format of imx8m series gpt?

I'm currently using the images in LF_v5.15.5-1.0.0_images_iMX8MPEVK, but the partition format is configured as MBR.

Q2) Why is the LF_v5.15.5-1.0.0_images_iMX8MPEVK image configured with MBR? Do you have a reason?

Q3) Is it possible to change from MBR to GPT? Any problems?

Q4) Where should I modify to change from MBR to GPT?

0 Kudos
Reply
1 Solution
2,387 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
Reply
4 Replies
2,388 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Q)How to change the partition format from MBR to GPT?
[Ans]:

The default partition format of the i.MX8M series is MBR.
It is possible to change from MBR to GPT.
You should modify the wks file in yocto to change from MBR to GPT.

One can refer to 4.1 Partitioning at the image creation stage in AN13706.pdf (Partitioning the Storage Medium on the i.MX 8M Family).

 
Thanks & Regards,
Dhruvit Vasavada
0 Kudos
Reply
2,358 Views
Y_K
Contributor I

Hi,  @Dhruvit 

Sorry for the late reply.

I tried reading the document you provided.
Solved without incident.

thank you very much.

0 Kudos
Reply
2,341 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Y_K,

I hope you are doing well.

Glad to know that issue is resolved.

Can I mark this case as close?

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply
2,336 Views
Y_K
Contributor I

Hi, @Dhruvit 

>Can I mark this case as close?
   Yes, it is okay.
   thank you very much.

0 Kudos
Reply