How to change EPD Waveform(WBF) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change EPD Waveform(WBF) ?

Jump to solution
3,843 Views
hiroyukihara
Contributor III

Development environment
 Development Board   MCIMX6DL-SDB
 EPD Daughter card   IMXEBOOKDC4-EPD
 OS          Android 7.1

When changing from 6 inch EPD attached to IMXEBOOKDC4-EPD to 13.3 inch EPD,
Where will you write Waveform (WBF) for 13.3 inch?

(E-Ink 13.3inch  320_R066_AD5901_ES133UT2C1_TC.WBF)
Please tell me how to change Waveform (WBF).

Thanking you in advance.

0 Kudos
Reply
1 Solution
3,518 Views
art
NXP Employee
NXP Employee

Actually, the software by NXP does not use the .wbf waveform file, provided by the EPD vendor, but uses a custom .fw waveform file. So, you have to provide the original .wbf file to us so that we will convert it to the corresponding .fw file. Please refer to the Chapter 10 of the attached document for the information on how to integrate a custom .fw file into the software.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,519 Views
art
NXP Employee
NXP Employee

Actually, the software by NXP does not use the .wbf waveform file, provided by the EPD vendor, but uses a custom .fw waveform file. So, you have to provide the original .wbf file to us so that we will convert it to the corresponding .fw file. Please refer to the Chapter 10 of the attached document for the information on how to integrate a custom .fw file into the software.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply