Development environment
Development Board MCIMX6DL-SDB
EPD Daughter card IMXEBOOKDC4-EPD
OS Android 7.1
When changing from 6 inch EPD attached to IMXEBOOKDC4-EPD to 13.3 inch EPD,
Where will you write Waveform (WBF) for 13.3 inch?
(E-Ink 13.3inch 320_R066_AD5901_ES133UT2C1_TC.WBF)
Please tell me how to change Waveform (WBF).
Thanking you in advance.
已解决! 转到解答。
Actually, the software by NXP does not use the .wbf waveform file, provided by the EPD vendor, but uses a custom .fw waveform file. So, you have to provide the original .wbf file to us so that we will convert it to the corresponding .fw file. Please refer to the Chapter 10 of the attached document for the information on how to integrate a custom .fw file into the software.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Actually, the software by NXP does not use the .wbf waveform file, provided by the EPD vendor, but uses a custom .fw waveform file. So, you have to provide the original .wbf file to us so that we will convert it to the corresponding .fw file. Please refer to the Chapter 10 of the attached document for the information on how to integrate a custom .fw file into the software.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------