Hello,
I'm working with IMX6ULL and I'm trying configure SDMA in ecspi1, but without success.
this is my configuration in device tree:
&sdma {
compatible = "fsl,imx6ull-sdma";
reg = <0x020ec000 0x4000>;
interrupts = <GIC_SPI 2 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_SDMA>,
<&clks IMX6UL_CLK_SDMA>;
clock-names = "ipg", "ahb";
#dma-cells = <3>;
iram = <&ocram>;
fsl,sdma-ram-script-name = "imx/sdma/sdma-imx6q.bin";
};
&ecspi1 {
fsl,spi-num-chipselects=<1>;
cs-gpios = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";
dmas = <&sdma 3 7 1>, <&sdma 4 7 2>;
dma-names = "rx", "tx";
spidev@0x00 {
compatible = "spidev";
spi-max-frequency = <60000000>;
reg = <0>;
};
};
This configuration is correct? Someone have made this before?
Thanks.