How to cancel the interface movement while holding down the mouse in the weston graphical interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to cancel the interface movement while holding down the mouse in the weston graphical interface?

ソリューションへジャンプ
3,327件の閲覧回数
783435100
Contributor III

Dear technical support:   

   I use vdkEGL to develop a graphical interface, but I need to hold down the mouse and move to implement the object dragging function, but it is now used by the default main window. How to cancel it?

0 件の賞賛
返信
1 解決策
3,309件の閲覧回数
783435100
Contributor III

i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) CPU Board

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,315件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Could you tell me which product are you using?

Which board support package are you using?

0 件の賞賛
返信
3,308件の閲覧回数
783435100
Contributor III

imx-yocto-L5.4.47_2.2.0

DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source imx-setup-release.sh -b build-wayland

bitbake imx-image-multimedia

0 件の賞賛
返信
3,310件の閲覧回数
783435100
Contributor III

i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) CPU Board

0 件の賞賛
返信