Dear technical support:
I use vdkEGL to develop a graphical interface, but I need to hold down the mouse and move to implement the object dragging function, but it is now used by the default main window. How to cancel it?
Solved! Go to Solution.
i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) CPU Board
View solution in original post
Could you tell me which product are you using?
Which board support package are you using?
imx-yocto-L5.4.47_2.2.0
DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source imx-setup-release.sh -b build-wayland
bitbake imx-image-multimedia