How to cancel the interface movement while holding down the mouse in the weston graphical interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to cancel the interface movement while holding down the mouse in the weston graphical interface?

Jump to solution
930 Views
783435100
Contributor III

Dear technical support:   

   I use vdkEGL to develop a graphical interface, but I need to hold down the mouse and move to implement the object dragging function, but it is now used by the default main window. How to cancel it?

0 Kudos
1 Solution
912 Views
783435100
Contributor III

i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) CPU Board

View solution in original post

0 Kudos
3 Replies
918 Views
jimmychan
NXP TechSupport
NXP TechSupport

Could you tell me which product are you using?

Which board support package are you using?

0 Kudos
911 Views
783435100
Contributor III

imx-yocto-L5.4.47_2.2.0

DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source imx-setup-release.sh -b build-wayland

bitbake imx-image-multimedia

0 Kudos
913 Views
783435100
Contributor III

i.MX 8QuadXPlus Multisensory Enablement Kit (MEK) CPU Board

0 Kudos