How to add ubuntu roof file system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add ubuntu roof file system

1,835 Views
jiye
Contributor V

I am using bitbake core-image-base to build a new image file. I know I can flash the .sdcard image file directly. However, the roof file system on this image is basic. And it does not have apt-get as ubuntu does. I wonder how and if I can manually replace the roofts with ubuntu rootfs and the rest remain the same since ubuntu has its own apt-get repository. If this is possible, what kind files do I need to manually put into the two partitions of my SD card.

for example: something such as :

Linux OS kernel image (zImage/Image)

Device tree file (*.dtb) • Bootloader image 

Root file system (i.e., EXT4) (with ubuntu root file system)

I am really confused about what files and format (eg. uboot.img?) exactly I need to put in partition one and partition two(rootfs.gz?).

2 Replies

1,696 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jiye

one can look on

https://developer.solid-run.com/knowledge-base/i-mx8m-debian/ 

https://boundarydevices.com/wiki/debian-for-nitrogen8/ 

https://community.nxp.com/thread/325384 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,696 Views
jiye
Contributor V

the first link you gave me it's for i-mx8m not for mini right ? I tried on my mini eva there is no response from there.

0 Kudos
Reply