Hi Community,
I am using imx6 with our custom board, and trying to use dual display (LVDS+HDMI).
kernel version -4.1.15
X11(xserver) version-1.18.0
Vivante (Galcore) - 5.0.11
I know accelerated dual display is not possible with imx6 (Kernel 4.1.15). its limitation.
see iMX6 Accelerated Dual-Display with X11 and Vivante Driver Segfault
How can i use one accelerated and one without acceleration ?
Xserver recipes -
My xorg,conf is as below
==================================================================
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device 0"
Driver "vivante" // tried with fbdev driver and Noaccel option but not working.
Option "fbdev" "/dev/fb0"
Option "vivante_fbdev" "/dev/fb0"
Option "HWcursor" "false"
EndSection
Section "Device"
Identifier "i.MX Accelerated Framebuffer Device 1"
Driver "vivante"
Option "fbdev" "/dev/fb2"
Option "vivante_fbdev" "/dev/fb2"
Option "HWcursor" "false"
EndSection
Section "Screen"
Identifier "LCD"
Device "i.MX Accelerated Framebuffer Device 0"
Monitor "Monitor_0"
DefaultDepth 16 #Choose the depth (16||24)
SubSection "Display"
Depth 16
Modes "800x480_60.00" #Choose the resolution
EndSubSection
EndSection
Section "Screen"
Identifier "HDMI"
Device "i.MX Accelerated Framebuffer Device 1"
Monitor "Monitor_1"
DefaultDepth 16 #Choose the depth (16||24)
SubSection "Display"
Depth 16
EndSubSection
EndSection
Section "Monitor"
Identifier "Monitor_1"
EndSection
Section "Monitor"
Identifier "Monitor_0"
EndSection
Section "ServerLayout"
Identifier "Default Layout"
Screen 0 "LCD"
Screen 1 "HDMI" RightOf "LCD"
#InputDevice "hy462x" "Pointer"
#InputDevice "eGalaxTouch" "Pointer"
Option "Xinerama" "on"
EndSection
Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection
=======================================================
Please let me know how it is possible ?
Any help would be highly appreciated ?
Regards,
Pankaj
已解决! 转到解答。
Hi Bio_TICFSL,
Thanks for your response.
We have found another solution for that.
1. Create two users except root.(usr1 and usr2)
2. Change /dev/galcore permisssion as it is only accessible to usr1 and root, not accessible to usr2.
3. /dev/galcore is only accessible to root and one user(usr1) not to usr2.
4. Start first application with one user(usr1) who have access of /dev/galcore and second display with the user who have no access rights(usr2) on /dev/galcore.
5. Now Everything is working fine.
Regards,
Pankaj
Hi ,
It will works if you have two displays that are already working, but both are not working with gpu/vpu( with acceleration ) in that case you have to use this workaround. the workaround is based on primary display(with GPU/VPU) and secondary display(without GPU/VPU).
Launching application on dual displays using workaround will not crash your xorg.conf.
do not directly copy my xorg.conf, maybe it will not work for you, it will depend on which one is your primary display and which one is your secondary display, accordingly you have to setup your xorg.conf.
Regards,
Pankaj
Hi Bio_TICFSL,
Thanks for your response.
We have found another solution for that.
1. Create two users except root.(usr1 and usr2)
2. Change /dev/galcore permisssion as it is only accessible to usr1 and root, not accessible to usr2.
3. /dev/galcore is only accessible to root and one user(usr1) not to usr2.
4. Start first application with one user(usr1) who have access of /dev/galcore and second display with the user who have no access rights(usr2) on /dev/galcore.
5. Now Everything is working fine.
Regards,
Pankaj