How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

2,208件の閲覧回数
gurumoorthirasi
Contributor IV

Dear All,

I am using i.mx25 processor for our application.I am using Linux 2.6.31 with freescale BSP for i.mx25. we require RTC for our application.

Any one tel me what are changes involved in kernel 2.631 to add RTC(Ds1307) and work it up.

Regards,

Guru

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,899件の閲覧回数
b36401
NXP Employee
NXP Employee

Please refer to section 26.5 "Programming Interface" of attached Linux manual regarding to supported RTC API functions for i.MX25 processor.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信