How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

2,094 次查看
gurumoorthirasi
Contributor IV

Dear All,

I am using i.mx25 processor for our application.I am using Linux 2.6.31 with freescale BSP for i.mx25. we require RTC for our application.

Any one tel me what are changes involved in kernel 2.631 to add RTC(Ds1307) and work it up.

Regards,

Guru

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,785 次查看
b36401
NXP Employee
NXP Employee

Please refer to section 26.5 "Programming Interface" of attached Linux manual regarding to supported RTC API functions for i.MX25 processor.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复