How to Enable PCIe in imx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Enable PCIe in imx6Q

2,428 Views
zohanlin
Contributor IV

Dear guys,

My kernel is v4.9.88 and my board is i.MX6Q.

I refer the link in NXP

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6Q-PCIe-EP-RC-Validation-System/ta-p...

 

For enabling PCIe function in imx6Q, I have three questions.

1. Do I need to enable CONFIG_RC_MODE_IN_EP_RC_SYS=y if I want plug a EP mode PCIe device to imx6Q?

2. Are the CONFIG_RC_MODE_IN_EP_RC_SYS &  the CONFIG_EP_MODE_IN_EP_RC_SYS only for testing R/W speed between two i.MX boards?

3. Do I need to enable cache for PCIe function in normal case? If yes, how to enable cache for PCIe?

 

Thanks,

zohan

Tags (3)
0 Kudos
Reply
4 Replies

2,425 Views
igorpadykov
NXP Employee
NXP Employee

Hi Zohan

 

1. please use option on that link

"Software configurations
* When building RC image"

2. no

3. suggested to use default dts:

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6q-sabresd.dts?h=imx_...

 

Best regards
igor

 

 

 

 

0 Kudos
Reply

2,402 Views
zohanlin
Contributor IV

Hi igor,

I plugged SIMCOM 5G module(EP mode) to i.MX6Q board, 

the PCIe read speed is 1.8 MB/s,  write speed is 7.8 MB/s.

 

I see the i.MX6Q spec it says the i.MX6Q support PCIe 2.0

Why the speed is slower than PCIe Gen 1?

 

I also done the same test on i.MX6QP EVB without externel OSC.

And the result is almost same as i.MX6Q.

 

Do you have any suggestion about my problem?

 

Thanks,

zohan

 

0 Kudos
Reply

2,396 Views
igorpadykov
NXP Employee
NXP Employee

bad performance may be due to noisy signals, one can try steps provided in AN4784 and

check if signal quality is good

AN4784: PCIe Certification Guide for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite - Application Note

 

Best regards
igor

 

 

0 Kudos
Reply

2,363 Views
zohanlin
Contributor IV

Hi igor,

We don't have those test equipments.

And we have test two 5G modules on i.MX6QP EVB: 

(1)SIMCOM SIM8202G-M2

(2)QUECTEL RM502Q-AE

SIMCOM & QUECTEL both have bad upload & download speed.

Their upload speed is about 2MB/s and download speed is about 6MB/s.

Do you have any idea about the issue?

0 Kudos
Reply