IMX6DP and hdmi display edid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6DP and hdmi display edid

1,010 次查看
vaudoitlaurent
Contributor IV

Hi,

on a imx6dp board,  we plug a hdmi display, and we get 640*480 resolution after boot, even if bootargs specify 1920*1080, and also the resolution of the screen is 1920*1080.

We use Yocto Warrior, kernel 4.19, from NXP release.

After some debug, i see that when the edid is read, the nearest mode (of 1920*1080) in the list found is 640*480.

Edid seems not embedding cea modes, and it seems the problem is coming from here.

 

I'm not sure the pb is coming from the EDID or from the board.

 

EDID read is the following:

0x00 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0x00 0x22 0x64 0xB0 0x04 0x00 0x00 0x00 0x00 0x28 0x1E 0x01 0x04 0xA0 0x1C 0x0F 0x78 0x02 0x98 0x74 0xA2 0x54 0x4B 0x9E 0x27 0x0C 0x4B 0x4F 0x00 0x00 0x00 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0xEA 0x38 0x80 0xF0 0x70 0x38 0x2C 0x40 0x30 0x20 0x36 0x00 0x1B 0x9F 0x10 0x00 0x00 0x18 0x00 0x00 0x00 0x10 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0xFE 0x00 0x48 0x61 0x6E 0x6E 0x53 0x74 0x61 0x72 0x0A 0x20 0x20 0x20 0x20 0x00 0x00 0x00 0xFE 0x00 0x31 0x32 0x38 0x4A 0x55 0x57 0x31 0x2D 0x43 0x31 0x30 0x0A 0x20 0x00 0xF4 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00

 

 

Thanks in advance for your support.

Regards

Laurent

0 项奖励
回复
1 回复

998 次查看
vaudoitlaurent
Contributor IV

Hi,

any feedback on this topic?

 

regards

Laurent

0 项奖励
回复