How to Add packages to rootfs on gui?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Add packages to rootfs on gui?

1,171 Views
erenbasturk
Contributor II

Hi, I couldn't find that how can I add package to rootfs on a GUI. I have no problem with addign package to local.conf but I need a GUI like buildroot.

As I see, yocto doesn't support HOB on the latest version. Do you have any suggestion?

Best Regards,

Eren

0 Kudos
Reply
2 Replies

987 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Eren,

You may still use HOB. It is deprecated but still working and will no longer be available in Poky 2.1 in favor of Toaster, which does not still have the same functionalities of HOB.  If you are using the Community BSP you should have no problem using HOB. Some problems were detected in Daisy for the BSP Release, with some posts in these communities showing some workarounds. I would recommend trying using it as this is the only GUI available for recipe customization as of today.

Regards,

0 Kudos
Reply

987 Views
erenbasturk
Contributor II

Any suggestion?

0 Kudos
Reply