How to Add packages to rootfs on gui?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Add packages to rootfs on gui?

1,170件の閲覧回数
erenbasturk
Contributor II

Hi, I couldn't find that how can I add package to rootfs on a GUI. I have no problem with addign package to local.conf but I need a GUI like buildroot.

As I see, yocto doesn't support HOB on the latest version. Do you have any suggestion?

Best Regards,

Eren

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

986件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Eren,

You may still use HOB. It is deprecated but still working and will no longer be available in Poky 2.1 in favor of Toaster, which does not still have the same functionalities of HOB.  If you are using the Community BSP you should have no problem using HOB. Some problems were detected in Daisy for the BSP Release, with some posts in these communities showing some workarounds. I would recommend trying using it as this is the only GUI available for recipe customization as of today.

Regards,

0 件の賞賛
返信

986件の閲覧回数
erenbasturk
Contributor II

Any suggestion?

0 件の賞賛
返信