How many camera inputs can be used in IMX6 Quad simultaneously?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many camera inputs can be used in IMX6 Quad simultaneously?

ソリューションへジャンプ
3,432件の閲覧回数
ivyliu
Contributor IV

Hi,

I am now using IMX6 Quad.

I know it support 2 parallel ports and 1 MIPI port.

IMX6 Quad has 2 IPUs.

Could you please tell me can it use these 3 ports simultaneously?

If it can, is it right that  MIPI and 1 parallel use 1 IPU and the other parallel use another IPU?

Thank you very much!

Best Regards,

Ivy

ラベル(3)
1 解決策
2,995件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6Quad processor has three camera ports, physically routed out of the chip: two parallel ones (IPU1_CSI0 and IPU2_CSI1) and one MIPI CSI. The MIPI CSI port input can be routed to any of the two IPUs with so-called MIPI_CSI-to-IPU gasket module. And, yes, you can use all these three ports simultaneously.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,996件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6Quad processor has three camera ports, physically routed out of the chip: two parallel ones (IPU1_CSI0 and IPU2_CSI1) and one MIPI CSI. The MIPI CSI port input can be routed to any of the two IPUs with so-called MIPI_CSI-to-IPU gasket module. And, yes, you can use all these three ports simultaneously.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,995件の閲覧回数
ivyliu
Contributor IV

Hi Igor and Artur,

Thank you very much for the prompt reply!!

Best Regards,

Ivy

0 件の賞賛
返信
2,995件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

you are right: two IPUs and each has two CSI :

1.jpg

In general you can connect 4 cameras to the MIPI CSI-2 interface.

For this you have to multiplex the four streams in an FPGA.

Each camera in this case should use a different stream

identifier (stream 0-3),  4 data streams can the be distributed across

the 4 CSI.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,995件の閲覧回数
ivyliu
Contributor IV

Hi Igor,

Thank you very much for your prompt reply!!

Best Regards,

Ivy

0 件の賞賛
返信