How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

跳至解决方案
1,293 次查看
zengzhaoping
Contributor II

my board is imx6q and the kernel version is imx3.10.53;the default max scaling frequency is 996000HZ;

but the document saild ldo mode is support 1.2GHZ,I do not know how to achieve。

when I decode video ,I nead the max scaling frequency ,can you help me? thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,108 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,109 次查看
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复