How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

ソリューションへジャンプ
1,287件の閲覧回数
zengzhaoping
Contributor II

my board is imx6q and the kernel version is imx3.10.53;the default max scaling frequency is 996000HZ;

but the document saild ldo mode is support 1.2GHZ,I do not know how to achieve。

when I decode video ,I nead the max scaling frequency ,can you help me? thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,102件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,103件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信