How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How increasing the iMX6q ARM cores max scaling frequency to 1.2GHz?

Jump to solution
1,308 Views
zengzhaoping
Contributor II

my board is imx6q and the kernel version is imx3.10.53;the default max scaling frequency is 996000HZ;

but the document saild ldo mode is support 1.2GHZ,I do not know how to achieve。

when I decode video ,I nead the max scaling frequency ,can you help me? thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,123 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhaoping

software automatically supports 1.2GHz checking fuse SPEED_GRADING,

note one needs to use 1.2GHz grade parts, like MCIMX6Q5EYM12AC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply